Views:
          
About Delta
Delta, founded in 1971, is a global leader in power and thermal management solutions. Our mission is “To provide innovative, clean and energy-efficient solutions for a better tomorrow,” and our businesses encompass Power Electronics, Energy Management, and Smart Green Life. Delta has sales offices, manufacturing facilities and R&D centers worldwide. In 2014, ranked at the highest A-level of the Climate Performance Leadership Index of the Carbon Disclosure Project (CDP). Since 2011, Delta is part of the Dow Jones Sustainability Indices (DJSI) World Index.
 
Grid power technical specification for grid provider of full 16 power units requested by grid provider, in Norway, including rise and fall value ΔPΔt:

Solution

Table 1. 

 Charger Type EVC 200 kW 3IN1 H0-AH-LW0EK-0000
 Maximum effect/charger [kW] 215 kW
 Maximum effect/charger [kVA] S= ~215 kVA (range of power factor is 0.98-0.99)
 Rectifier, type of (e.g 6-pulse, 12 pulse)? rectifier is built as 3x1-phase rectifiers (full bridge, two pulses), each stage has   separate PFC.
 Rectifiers How many? 16 pcs
 Effect change per time unit kW/s Max response speed (normal operation): Rise 384+19 kW/s Descend 961+19 kW/s
 Reverse feeding  No

 

 

 
 
 
 

Disclaimer Notice
By using Delta Electronics (Netherlands) B.V. and affiliates website and its technical information, you agree to be bound by the terms of this warranty disclaimer.