Views:
          
About Delta
Delta, founded in 1971, is a global leader in power and thermal management solutions. Our mission is “To provide innovative, clean and energy-efficient solutions for a better tomorrow,” and our businesses encompass Power Electronics, Energy Management, and Smart Green Life. Delta has sales offices, manufacturing facilities and R&D centers worldwide. In 2014, ranked at the highest A-level of the Climate Performance Leadership Index of the Carbon Disclosure Project (CDP). Since 2011, Delta is part of the Dow Jones Sustainability Indices (DJSI) World Index.

Technical note

1. Remotely ask the customer for the log file.

2. Locally on-site download the log file with a USB stick.

3. The following is a list of parts based on the spare parts list for the 3G modem:

  • The module Huawei 609 is the first 3G module manufactured with the DCWB (Old generation 3G modem)
  • The module Huawei 709 Is the second module manufactured with the DWCB (New generation 3G modem)
  • Both modules are compatible with all FW on DCWB (from V01.30 to V02.05)

Figure 1. Huawei 609 Old generation 3G modem part number 3798100045-S


 

Figure 2. Huawei 709 New generation 3G modem part number 3798101746-S


 

4. It is possible to see if the module is a 3G module or not based on the log files:

Figure 3. Log files

5. The following is a list of parts based on the spare parts list for the 4G modem:

  • If the module PLS83-W is mentioned it means a 4G module is installed (at this moment only model PLS83-W is proposed). 
  • This module is only compatible with a KIT 4G as mentioned in KA-100003430.

Figure 4. 4G module part number 5505606568-S

 

6. It is possible to see remotely if the module is a 4G module or not based on the log files.

Figure 5. 4G module example log files

 

7. It is normally possible to identify the module model based on its label.

Figure 6. Example module model label (MU709s-6 - new gen 3G)

 
 
Disclaimer Notice
By using Delta Electronics (Netherlands) B.V. and affiliates website and its technical information, you agree to be bound by the terms of this warranty disclaimer.